Hello!
I have a problem, completely similar in topic:
I check all connections, and found difference between two schematics:
If i connect like Figure 9, CC Debugger and RF Studio found CC1125. Continuous RX and Continuous TX work properly, but i have problem only with Packet TX/RX modes (Rf Control Panel says:"Radio State N. A".
If i connect like on Figure 8, CC Debugger not found CC1125.
Difference with connection GPIO0 and GPIO2. Which connection diagram is correct?
My reference board powered from CC Debugger. Pin 2 connect to pin 9 on the CC debugger connector.
Best regards, Alex.