Tool/software: Code Composer Studio
Dear Sir,
This is an emergency case.
I bought a CC1310 module from some third-party vendor.
I used the TI CC1310 launchpad as the JTAG debugger (by removing some jumpers from launchpad, and connect a JTAG
cable to the third-party CC1310 module).
At beginning, I tried to program it by using CCS, however, CCS complained that it is "write protected".
So, I turned to use TI flash programmer 2 to execute a "mass erase". Then I can program it with my
image (.out file) by CCS.
The programming process looked good, and it ran well after pressing CCS "play" button.
However, when I tried to reboot and free-run the module (without XDS debugger), it seemed not running as I saw no packet
emitted from the module by packet sniffer's view.
I doubt that if the image really being programmed into the flash.
Then, I used the XDS debugger to launch it again without loading program, but just loading symbol tables only,
after doing run-> Reset -> System Reset, the module ran successfully again.
Q1: What is the key of my trouble? Is it related to bootloader?
Q2: I doubt if the "Mass Erase" erased the bootloader too. Is it true?
Q3: Does the .out image file contain bootloader?
Thank you for your help
BR,
Adam