This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

SIMPLELINK-CC13X2-26X2-SDK: simplelink_cc13x2_26x2_sdk_4_10_00_78

Prodigy 100 points

Replies: 1

Views: 81

Part Number: SIMPLELINK-CC13X2-26X2-SDK

When I use IAR to open the SDK project, I get the following error. IAR embedded workbench 8.32, 8.42 and 8.50 all have the same error report. The SDK version is simplelink_ cc13x2_ 26x2_ sdk_ 4_ 10_ 00_ 78 and simplelink_ cc13x2_ 26x2_ sdk_ 3_ 40_ 00_ 02. Previous versions of SDK do not report errors.

Building configuration: i2ctmp_CC1312R1_LAUNCHXL_tirtos_iar - Debug
Updating build tree...

0 file(s) deleted.
Updating build tree...
Performing Pre-Build Action
Error while running iarbuild.exe c:/ti/simplelink_cc13x2_26x2_sdk_4_10_00_78/kernel/tirtos/builds/CC1312R1_LAUNCHXL/release/iar/tirtos_builds_CC1312R1_LAUNCHXL_release.ewp Debug -log all

Total number of errors: 1
Total number of warnings: 0

Build failed.

 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.