Hello there !
I would like to ask about the possibility of making a Mesh network with 6LowPAN and ISM band thread (920MHZ).
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello there !
I would like to ask about the possibility of making a Mesh network with 6LowPAN and ISM band thread (920MHZ).
Thank you.
Hi Amine,
It is possible but there is no Sub1G stacks in the current SDK delivery that supports Mesh at all (however there is some 2.4GHz stacks that could). You would need to implement this yourself, an alternative is to look at the Contiki-NG project on GitHub.
Hey !
Actually I don't need a Linux server so Contiki-NG project is not a good option for me,my main project is to make a sub1G mesh network and I thought TI provides a protocol for that.
So what I want to do is sending and receiving data between several nodes which is a MAC address and then I will try to classify the MAC so the nodes will know their mode either it will act like a master or a slave.
Thank you.
BR
Hi Amine,
As mentioned above, we do not provide any Sub1G mesh stack as the Sub1G stacks we over is focused on low-power. We do however provide a lot of details on how to work with the radio without any stack so that you can implement your own protocol on top of that.
Thank you,
Could you please provide these details so I can start working with the radio
BR
Hi Amine,
There is not really more details to this than what you could potentially get from the thread YiKai linked in here, and that is assuming you go with the TI 15.4 stack.
For your own custom implementation, it is recommended to look at the basic "rfPacketTx/Rx" examples on how to use the radio and then code away from there.