Hello,
I have been evaluating the TI15.4 example code. I wanted to find out what is the minimum reporting interval for which 0 packet loss can be attained. I have been testing the Collector example with the sensor example based on sdk 3.20.23, with a reporting interval of 1000ms, 433mhz and FH enabled. I had connected 8 sensors to a single collector and I am observing a packet loss anywhere between 10% to 35% for a period of 8 hours.
Is this normal? How does this compare to the official TI numbers? Also at what minimum reporting interval can I get minimal packet loss(Ideally 0 packets lost) ?
Regards
Sabin