Other Parts Discussed in Thread: CC1310, CC1190
hi,
referring to the screen shots below, i used smartrf studio to generate continuous modulated data on a standard cc1310 launchpad versus a cc1310-1190 launchpad.... with my rf-explorer consistently placed 6" from the antenna, here's what i see....
in general, the cc13-90 is somewhat lower than the cc1310 baseline; perhaps this is differences in the antenna????
i also captured the cc13-90 transmitting at 26dB.... and while the signal is definitely stronger, i somehow expected more....
to be fair, i haven't attached an external antenna to the cc13-90....
any suggestions, or is this the best i can achieve???
bob.