Tool/software: Code Composer Studio
Hi,
I am using the rfWakeOnRadioRx and rfWakeOnRadioTx example in SDK ,and I want to know the connection distance of them.
At the time of my test, their communication distance was only 40 meters.What is the problem? and how to extend the communication distance?
The following is the smart setting:
*** // Parameter summary // RX Address0: 0xAA // RX Address1: 0xBB // RX Address Mode: No address check // Frequency: 433.00000 MHz // Data Format: Serial mode disable // Deviation: 25.000 kHz // Packet Length Config: Variable // Packet Length: 20 // Packet Data: 255 // RX Filter BW: 98 kHz // Symbol Rate: 50.00000 kBaud // Sync Word Length: 32 Bits // TX Power: 15 dBm (requires define CCFG_FORCE_VDDR_HH = 1 in ccfg.c, see CC13xx/CC26xx Technical Reference Manual) // Whitening: No whitening
Regards,
Kevin