Other Parts Discussed in Thread: CC1101, CC1190
Hi,
we use a Sky FEM as single PCB device usually for boosting TX in certain applications to up to 30dB (SKY 66119).
This chip has RX boost too, but when I try to gain more RX sensivity I fail:
Typical test bed: RF generator -> CC1120 -> BER test --->> ~ -120dBm (transparent mode)
The FEM has a RX gain of ~15dB, this is what I can verify if I measure the output in a test bed like:
RF generator -> FEM -> spectrum analyzer (SA) --->>> the input at SA is 15dB higher the the output of the generator, this is what I expect. E.g. -125dBm input, -110dBm output
But in verify mode:
RF generator -> FEM -> CC1120 -> BER test the BER is the same BER than without the FEM, ~ -120dBm
Thats where I struggle: do I oversee something or any other hint?
Or: to what extend a FEM can boost sensivity in real world?
thx.