We have a setup with an application that is using OAD. For programming, the hex file is merged with the BIM
Now, both the BIM and the application have CCFG settings in the code in much the same way.
Can I safely assume that only the CCFG of the BIM is used and the CCFG of the application is ignored?
Or do I have to make changes to accomplish this?