Tool/software: TI C/C++ Compiler
Hi guys,
Im using cc1350 launchpad microprocessor , and sending packet in Long Mode Range 1 , the parameters that Im configuring shown down in the attached photo:
I transmit those packets LRM and I want to capture those packets as IQ samples .
I use dongle for sampling the transmitted packets, and the IQ samples I see them in matlab.
As shown in the photo in my case the DSSS=8 , this means according to:
if there's 0 then it will be mapped to 11001100 , and 1 will be mapped as 00110011.
So what's confusing me that I I built a demodulator, then I should see on the output of my demodulator my packets data in terms of DSSS=8 (in other words in terms of 11001100 or 00110011) , am I right?
before doing the decoder or encoder, I must verify in my demodulator that on its outputs I see my packets in terms of DSSS=8, for instance I should see my syncword in terms of 11001100 or 00110011 ..right?!
A pleasure for any help.