Other Parts Discussed in Thread: CC1352R, LPSTK-CC1352R, TPS61023, TPS22910A
Hi,
I'm going to design my custom board using 2XAA(2S) batteries similar to below diagram.
Do you have any reference design files? or any recommends?
Thanks in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm going to design my custom board using 2XAA(2S) batteries similar to below diagram.
Do you have any reference design files? or any recommends?
Thanks in advance.
Hi,
Have you seen this ref design that utilizes two 2xAA batteries to a CC1352R: https://www.ti.com/lit/zip/swrr170
Is it mainly the power conversion from AA batteries to 5V that you need info on ?
Regards,
Richard
Hi
Thanks for your information.
Yes, what I want to know was "the power conversion from AA batteries to 5V"
Q1. Do yo have any reference design for that?
Q2. What's your opinion about "TPS61222DCK" for the power conversion from 2xAA batteries to 5V?
Q3. What is the purpose of using "TPS22910AYZV(U7)" in the reference schematic you sent?
BR,
Kevin
Hi Kevin,
I will assign this thread to the power forum so they can answer your questions since this is not my field.
Regards,
Richard
Hi Kevin:
May I know what's the load condition?
Vin=2.5V, Vout=5V, right?
Hi, Minqiu
1. Here is condition.
- Vin : 2AA batteries(No rechargeable) => around 2.5V~3.3V
- Vout = 5V
- Load = under 500mA
2. Would you give me the answer on "Q2. What is the purpose of using "TPS22910AYZV(U7)" in the reference schematic(MCU071A_LPSTK-CC1352R_Schematic) you sent?"
Thanks in advance.
Kevin
Hi Kevin:
For such loading, you can have a look at TPS61023. It should be a good choice.
For the TPS22910, I suspect you are asking Richard.
Hi Richard:
May you help to answer this question? Thank you!
Thanks Minqiu,
Anyone can answer my questions below?
Q3. What is the purpose of using "TPS22910AYZV(U7)" in the reference schematic you sent?
Hi Kevin,
TPS22910A is an active low load switch. I am not extremely familiar with the design in question but it looks like the load switch is used to provide a controlled rise time after the battery is connected to avoid any output capacitances to pull large currents during turn on.
This is a common use of our load switches in the power stage.
Thank you for using TI Power Switches in your designs.
Hi, Shreyas.
That's what I want to know. Thanks.
Richard and Minqiu,
Once again, Thanks all of you
Kevin