Hi,
I use CC1352R with SDK simplelink_cc13x2_26x2_sdk_4_10_00_78.
The question is:
Is it possible to use function for dynamically enable/disable interrupt on single GPIO pin, from device specific gpio driver (simplelink_cc13x2_26x2_sdk_4_10_00_78\source\ti\devices\cc13x2_cc26x2\driverlib) or for this purpose
function from (C:\ti\simplelink_cc13x2_26x2_sdk_4_10_00_78\source\ti\drivers\GPIO.h) should be used.
For example: PIN_setInterrupt(....)
What is the correct way for dynamically enable/disable interrupt on pin, when the time is critical?
Best regrads,
Ilian