Hello TI Team,
We are developing a device which required to have the FOTA feature. (We can only use GSM for this, we cannot use the BLE or any other radio available within the CC1352).
I was thinking that the below steps will be correct or not to follow the process. (Below green part are done, and for the red part we required some help or suggestion from TI). And we have a GSM modem connected to CC1352 via UART and we are able to download the Hex file from our cloud.
1) To Make the Bin file ready using the OAD Image Tool. (Currently, we are using Hex file in our cloud, as Bin is not a good option to download via GSM modem due to some special characters)
2) To Receive the Hex from Cloud
3) To Store the Hex file in external Memory
For this, we have the SPI driver ready and we can store this HEX file to anywhere, but we want some hints on this like how to add the headers (as we are skipping the OAD process of TI)
4) To Trigger BIM with the new location from external memory. (I guess if above point3 will be cleared then we can trigger the BIM with the new image's location)
Basically, we are skipping the whole OAD process and want to run BIM with the hex file we received from the cloud.
Let me know if I missed anything or I required to provide more information.
Thanks,
Bhautik