Other Parts Discussed in Thread: CC1310
Tool/software: Code Composer Studio
Hi Sirs,
Recently, I developed a project which is related to ADC application.
The project invokes the 5 ADC related APIs (as shown at the bottom).
I found the code size increased about 3.1 KB (by observing the .map file) compared to remarking the calls.
As the CC1310 has only 128 KB internal flash size, I could not build successfully if OAD feature was also enabled.
Is it reasonable that the ADC library cost so much space? (A big lookup table inside the lib?)
Adam
Thank you
--------------
ADC_init();
ADC_Params_init();
ADC_open();
ADC_convert();
ADC_convertRawToMicroVolts();