Hi all,
I have some issue with the uart module of cc1310.
There are two uarts that i am using in my project in which one is emulated uart.
uart 1 - DIO 3, DIO 2 (emulated)
uart 2 - DIO 13, DIO 12
The uart1 is working good both RX and TX, but in the case of UART2 the read callback function is not working when it receives the data in its RX pin, but the TX is working good.
Is there anyone knows why its happening like this?
Thank you