I designed a circuit board that is a variant of the LAUNCHXL-CC1352P1 design, except I added a second SP3T switch in order to electronically control three antennas. See enclosed schematic & layout. Using SmartRF Studio, when I measure TX power @ 915Mhz on the LAUNCHXL-CC1352P1 board using the external SMA port (conducted RF measurement), the TX power level matches that of my board (on either ANT-2 or ANT-3). However, if I perform the same conducted RF measurement at 2.4GHz, my board is around 12dB worse. Any thoughts ?