Other Parts Discussed in Thread: CC1350
Hello sir,
i am using CC1350 launchpad and simplelink sdk with ti154stack (collector and sensor) examples. In this example collector device is starting the network by using the keypress(BUTTON1) and sensor device is joining by keypress(BUTTON1). Now i want to start the network and joining should be done at the time of device start for this i have enabled AUTO_START and NV_RESTORE options in preprocessor options in CCS by checking in collector.opt file. even though network is not started on device startup am i missing anything or do i need to do any changes to the code.
And i need to add the some adc code at sensor side. Is there any guide which will show the complete architecture/work flow of ti154stack for collector and sensor examples. please mention
thanks and regards