Replies: 24
Views: 538
Please provide info on what SDK you are using, what exact files you are referring to. What are you using the SmartRF06EB for?
BR
Siri
Try to refer to Restore to the factory image section in Meet the SimpleLink LPSTK-CC1352R LaunchPad SensorTag Development Kit.
If my post answers your question, please click on "This Resolved my issue" button to benefit others who have the same issue.
YK Chen
Comparision on Zigbee, Z-Wave, and Z-Wave Long range.
Build OpenThread Sleepy End Device doorlock prototype to test with Rasperry Pi OpenThread Border Router
How to use two UARTs in CC26x2 and CC13x2
SwitchBot DIY using LPSTK-CC1352R , SG90 servo motor, and ProjectZero to away from COVID-19.
How to use two endpoints in SIMPLELINK-CC13X2-26X2-SDK Z-Stack.
How to create a periodic event to toggle BLE Advertising in CC26xx simple_peripheral example
How to use indication in simple_peripheral example and use Btool to enable indication
How to detect button hold in CC26x2, CC13x0, CC13x2 SDK.
660 Zigbee devices in the same Zigbee network!
In reply to YiKai Chen:
In reply to Mario Castaldo:
If you build multi_sensor (: \CC1352R1_LAUNCHXL\ble5stack\multi_sensor) using CCS and download it to your LBSTK-1352R, can it work?
Does your LPSTK-1352R ever work after you receive it?
Do you restore to the factory image by pressing BTN-1 (left button) during a boot/reboot using the following steps?
I did this on my LPSTK-2652R and it can recover to factory image. If you debug multi_sensor example on CCS, can it stop in main function after you debug and download the code?