This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352R: CC1352R ASK(OOK) transmission

Part Number: CC1352R
Other Parts Discussed in Thread: CC1310, CC1312R, SYSCONFIG

Hi,

I would like to continue already closed thread-  https://https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz/f/156/t/576254?CC1310-OOK-mode-at-20-kbps

In ti topic: https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz/f/156/t/576254?CC1310-OOK-mode-at-20-kbps

The settings are for CC1310R and only the settings for bit rate are changed.

To use CC1352R for transmission of a OOK modulation on 433MHz with bit rate 19.2kbit/s , is this mean, that I should use RF setting from Smart RF Studio 7, which are for CC13510.

There is no section to enable ASK, when the CC1352R is used.

Best regards,

Ilian