Other Parts Discussed in Thread: WMBUS
Hello all,
Til now we used the Launchpad for testing the wMBusStack but now we are moving our code from the CC1310 LaunchXL to our custom Board with the CC1310.
Question 1: The Launchpad uses the CC1310F128, is this necessary for using the wMBus Stack or is it possible to use a CC1310F64 with the wMBus Stack?
I tried to reduce the size of the binary by changing the memory size and the project configurations as it is explained in this thread to the memory size
and in this thread to the project settings.
Afterwards in CCS when I want to build my wMBus program for a CC1310F64 the following error appeared:
"../cc13x0f64.cmd", line 91: error #10099-D: program will not fit into available memory. placement with alignment fails for section ".text" size 0xf722 . Available memory ranges: FLASH size: 0x10000 unused: 0xfae0 max hole: 0xeb10
Question 2: If it is possible to use the wMBus Stack on a CC1310F64, how can I reduce the size of the binary to 64kB? Is it possible to delete code or "tidy up" the memory allocation by avoiding wholes?
Thanks in advance