condition :
cc1310
SDK Version : simplelink_cc13x0_sdk_3_20_00_23
Use rfWsnNode example.
The transmitter sends a data packet every 60s.
There is no problem at normal temperature.
abnormal :
In an environment where the temperature changes rapidly high, system is rebooted continously.
If i block EasyLink_transmit() in NodeRadioTask.c, system is not rebooted.
Question :
What can i do to prevent the system from rebooting, in an environment where the temperature changes rapidly high ?