Hi ,
It’s the first time I try CC1312 with IAR v8.32.1.
I have a project that works fine with CC1310 , IAR v7.5
Now, it the new setup, I get the following Errors:
Error[Li060]: module "xdc_init.orm3(iar.targets.arm.rts.arm3)" contains C++ code built for use with the (E)C++98 library. This code is not link compatible with the new (C++14) library.
Fatal Error[Li001]: could not open file "C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.2\arm\lib\dlpp7M_tl_ne.a" (failed opening file: The system cannot find the file specified.
: iostream stream error)
Error while running Linker
Do you have any suggestion for solving it?
Thanks in advance
Eyal