The WOR cycle is 3S, the minimum is only Rx timeout is 2441ppm*3s 7.3ms. If the current 15.7ma, this power is too large.
The host sends data only send 2 bytes (leading) + 2 (synchronous character) +2 (address) + 1 (length) + 2 (CRC) =9 bytes, 9* /38.4K 1.875ms <7.3ms = 8.
Question 1:
when the host does not have data to send or the host does not send the corresponding address from the address of the data, how toreduce this time? Is the RSSI threshold and address matching check valid?
Question 2:
3s WOR state timeout can only be about 7.3ms., right?