Hello everyone!
First of all, this is my first post in this forum.
So, sorry if I make any mistakes.
I'm designing a wireless sensor powered by energy harvesting. So low current consumption is a must.
At this point, I developed a firmware that turns on the RF module in Rx mode for about 17ms and than turn it off and enter sleep mode for about 5s.
This development have been made using CC1310 Launchpad kit, where I could reach a average power consumption of about ~35uA, which is great for my needs!
The problem came after I have designed my custom PCB.
Everything is working almost fine.
RF module is working, but not as efficient as it should be.
This was expected since I have never worked with RF. (I will leave this topic for another post)
The most important fact right now is power consumption.
With this custom board, I could reach only ~70uA of average power consumption.
By reading some other posts in this forum, I believe the problem is on PCB layout.
As this is just a prototype board, its a 2 layer board, FR4.
The final design will be 4 layers.
Which are the critical components on the layout to reach the lowest possible power?
Is there any hints to lower this power consumption?
Thanks guys,