Part Number: CC1312R
Other Parts Discussed in Thread: CC1310
Hello!
Previously we used "Frequency Offset" on received packets feature with CC1310:
rfc_CMD_READ_RFREG_t RF_cmdReadRfregFreqOffset =
{
.commandNo = 0x0601,
.address = 0x5154,
.value = 0,
};
RF_runImmediateCmd(rfHandle, (uint32_t*)&RF_cmdReadRfregFreqOffset); offset = RF_cmdReadRfregFreqOffset.value;
With this offset information we could do a frequency calibration of nodes in network "on-the-fly".
Now we are moving to CC1312 and this command always returns "0".
Is the command 0x0601 still supported on new crystals?
Thank you!