This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Q: What is mioty?
A: A low-power wide area network that offers a complete long-range and low-power solution for worldwide Sub-1 GHz communication.
Q: How does the mioty technology compare to other LPWAN technologies ?
A: mioty is unique in the way it transmits data. Instead of sending it as one packet, mioty divides the telegram (data packet) into multiple sub-telegrams that are distributed in the time and frequency domains. This makes mioty more scalable and robust compared to other LPWAN technologies.
Q: What kind of range can I expect from mioty?
A: 5 km in urban and 15 km in rural environments.
Q: What’s the timeline for support of bi-directional communication?
A: The mioty stack from Stackforce already has support for bi-directional communication as well as the gateways from the different gateway providers.
Q: Where do I find information about the PHY and security features of mioty?
A: mioty is based on the telegram splitting ultra-narrow band (TS-UNB) family in the ETSI TS103358 standard. If you are interested in the technological details about the protocol, please refer to chapter 6 of the specification.
Q: What frequency bands are supported with mioty?
A: As described in the specification, the 868-MHz and 915- MHz frequencies are supported by the TS-UNB family.
Q: How does the licensing fee for mioty work?
A: There is an IP license cost related to using mioty, this is a one-time cost per device, which is handled by Sisvel. Refer to their website for more details.
Q: Can you share some technical details about the mioty low-cost gateway?
A: Here are the specifications for the mioty HAT reference design from Fraunhofer:
MIOTY Profiles |
EU0, EU1, EU2, US0 |
Frequency bands |
868 MHz, 915 MHz |
Sensitivity (EU1) |
< -135 dBm |
Blocking Dynamic Range (EU1) |
> 60 dB (100 kHz), > 90 dB (LTE20) |
Clipping-Free Dynamic Range (EU1) |
>91 dB |
TX Power |
14 dBm |
Connectors |
Raspberry PI GPIO |
Components for a functional base station |
Raspberry PI 4, CC1260, small FPGA, external LNA, power supply, and antenna |
Q: What are the key differences between the high-performance gateway and the low-cost gateway? Are there any differences in scalability?
A: The main difference is in the dynamic range and in the linearity. This will affect the receives ability to handle weak signals in the presence of other stronger wanted and/or unwanted signal. This could potentially influence the scalability, but from a signal processing side, there should be no difference with regards to scalability. The low-cost gateway is mainly intended for evaluation use, for indoor deployment or for rural areas whereas the high-performance gateway should be used for outdoor urban solutions.
Q: What gateways are currently on the market and what do they cost?
A: There are currently three mioty gateways on the market from Diehl, BehrTech and Weptech. Please visit the mioty store to see their offering and request a quote or contact the manufactures directly.
Q: How to get started?
A: In 4 easy steps (TI’s mioty Product folder):