CC1312R: The power consumption in boost mode on CC1312R

Guru 16610 points
Part Number: CC1312R

Hello,

Could you tell us the power consumption in the following conditions on CC1312R?
- VDDS = 2.1V (In case VDDS = 2.1V, we think CC1312R could output +14dBm)
- CC1312R is in boost mode

We can find the power consumption in the table 8.6 in the datasheet.
However, the figure seems to be only for VDDS = 3.6V.
We would like to know whether the power consumption is equal to the figure in the table in the above condition.

Best Regards,
Nomo