This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1271 suspend for DM3730 using WINCE

Other Parts Discussed in Thread: WL1271, DM3730

Hi,

   I am running with WL1271 on DM3730 using WinCE 6.0 R3. We can enable and disable the Wi-Fi interface  at the first time .When I  disable the Wi-Fi also into the sleep mode and Wi-Fi can't enable after wake up .The error message is below...

 

Texas Instruments Windows CE SD X-Loader for EVM 3730
Built Apr 20 2011 at 19:19:33
Version BSP_WINCE_ARM_A8 1.01.00.03
open ebootsd.nb0 file
Init HW: controller RST

SDCARD: reqested speed 1000000, actual speed 1000000

SDCARD: reqested speed 25000000, actual speed 19200000

jumping to ebootsd image

Microsoft Windows CE Bootloader Common Library Version 1.4 Built Apr 20 2011 19:16:54

Texas Instruments Windows CE EBOOT for OMAP35xx/37xx, Built Apr 20 2011 at 19:19:21
EBOOT Version 0.0, BSP BSP_WINCE_ARM_A8 1.01.00.03

TI OMAP3730 Version 0x00000012 (ES1.2)
TPS659XX Version 0x10 (ES1.1)
System ready!
Preparing for download...
INFO: Predownload....
Checking bootloader blocks are marked as reserved (Num = 14)

INFO: Boot configuration found

>>> Forcing cold boot (non-persistent registry and other data will be wiped) <<<
Hit space to enter configuration menu 5...
Hit space to enter configuration menu 4...
Hit space to enter configuration menu 3...
Hit space to enter configuration menu 2...
Hit space to enter configuration menu 1...
Init HW: controller RST
SDCARD: reqested speed 1000000, actual speed 1000000
SDCARD: reqested speed 25000000, actual speed 19200000
BLSDCardReadLogo:  cannot open Logo.bmp

BL_IMAGE_TYPE_BIN

Download file information:
-----------------------------------------------------------
[0]: Address=0x80002000  Length=0x027af57c  Save=0x80002000
-----------------------------------------------------------
Download file type: 1
......................................................................................................................................................................................................................................................................................rom_offset=0x0.
..ImageStart = 0x80002000, ImageLength = 0x27AF57C, LaunchAddr = 0x80012208

Completed file(s):
-------------------------------------------------------------------------------
[0]: Address=0x80002000  Length=0x27AF57C  Name="" Target=RAM
ROMHDR at Address 80002044h
Launch Windows CE image by jumping to 0x80012208...

Windows CE Kernel for ARM (Thumb Enabled) Built on Nov  3 2010 at 07:30:04
OAL: CPU revision 0x12:DM3730
OAL: CPU L2 Aux register 0x400042
****Profiler Build****
---High Performance Frequency is 26000288 hz---
Compensating OPP1 for 63mV Orig nvalue:0x99d3b6 New nvalue:0x99a790
Compensating OPP2 for 63mV Orig nvalue:0x9a81e0 New nvalue:0xaadec0
Compensating OPP3 for 75mV Orig nvalue:0xaab9a3 New nvalue:0xaaa28f
Compensating OPP4 for 100mV Orig nvalue:0xaa988a New nvalue:0xab84ee
ECC TYPE is Hamming 1 bit
DSPLINK Module (1.65.00.03) created on Date: Jan 17 2011 Time: 15:02:36
SDHC: CPU revision 0x12
SDHC host controller initialize: m_fastPathSDIO:1 m_fastPathSDMEM:0
 +++ HCI_OpenConnection +++
mode: 0x13
DRIVER_VERSION : 110, DATECODE : 041707
Rx PIO
Tx PIO
Lan9220 identified. ID_REV = 0x92200000
Use IntPhy
This chip doesn't support Auto Mdix!!!
HCI: Gpio2UartMode(): SetComPowerState,
set BRF as Wakeup source
 --- HCI_OpenConnection ---
+RunScript:brf61_7.2.31.bts
HCI: RunScript(): reach the end of script
HCI: -RunScript(): 1
TIWLAN: 0.005244: TI WLAN: DLL_PROCESS_ATTACH
TIWLAN: 0.005244: TIWL: DriverEntry In
TIWLAN: 0.005246: TIWL: DriverEntry Out
TIWLAN: 0.005251: TIWL: entryMiniportInitialize In

os_setDebugOutputToLogger set flag to 0
TIWLAN: 0.005284: AutoDetect = 0
TIWLAN: 0.005287: pInitParams->RoamingScanning_2_4G_enable 0
TIWLAN: 0.005359: wlanDrvIf_loadFile: name=n, handle=0x0, buffer=0xdec198a0, len=-557737820
TIWLAN: 0.005362: TIWL: Could not open image file, status=0xc001001b
TIWLAN: 0.005368: CHIP VERSION... set 1273 chip top registers
TIWLAN: 0.005375: Working on a 1273 PG 2.0 board.
TIWLAN: 0.005377: Starting to process NVS...
TIWLAN: 0.005381: No Nvs, Setting default MAC address
TIWLAN: 0.005386: pHwInit->uEEPROMCurLen: 1c
TIWLAN: 0.005390: ERROR: If you are not calibating the device, you will soon get errors !!!
TIWLAN: 0.005398: Chip ID is 0x4030111.
TIWLAN: 0.005402: wlanDrvIf_loadFile: name=F, handle=0x0, buffer=0xdec198a8, len=-557737812
TIWLAN: 0.005430: Starting to download firmware...
TIWLAN: 0.005525: Starting to download firmware...
TIWLAN: 0.005551: Starting to download firmware...
TIWLAN: 0.005551: Starting to download firmware...
TIWLAN: 0.005560: Starting to download firmware...
TIWLAN: 0.005564: Starting to download firmware...
TIWLAN: 0.005566: Finished downloading firmware.
TIWLAN: 0.005568: Firmware running.
TIWLAN: 0.005587:
TIWLAN: 0.005588: --------------------------------------------------------------------
TIWLAN: 0.005591: Driver Version  : WiLink_Driver_6.1.0.1.149
TIWLAN: 0.005596: Firmware Version: Rev 6.1.0.1.349
TIWLAN: 0.005601: Station ID      : 08-00-28-12-34-56
TIWLAN: 0.005606: --------------------------------------------------------------------
TIWLAN: 0.005613:
TIWLAN: 0.005630: Interrogate TX/RX parameters
TIWLAN: 0.005769: set OID_802_11_SSID |JUNK|
TIWLAN: 0.008806: set OID_802_11_SSID |JUNK|
touchp: calibration: new calibration data is "2060,1997 614,538 647,3480 3504,3487 3516,515 "
TIWLAN: 0.043335: TIWL: (SET)OID_PNP_SET_POWER 4
TIWLAN: 0.043335: TIWL: (SET)OID_PNP_SET_POWER NdisDeviceStateD3
kernel IOCTL_POWER_SET setting state 3
-OTG SetPowerState
Device Power State = NdisDeviceStateD3.
I2C: RESET device 12
kernel IOCTL_POWER_SET setting state 2
-OTG SetPowerState
kernel IOCTL_POWER_SET setting state 0
TIWLAN: 0.056063: TIWL: (SET)OID_PNP_SET_POWER 1
TIWLAN: 0.056143: wlanDrvIf_loadFile: name=n, handle=0x0, buffer=0xdec198a0, len=-557737820
TIWLAN: 0.056146: TIWL: Could not open image file, status=0xc001001b
TIWLAN: 0.056493: Try to SDBus Connect again...
TIWLAN: 0.056597: Try to SDBus Connect again...
TIWLAN: 0.056705: Try to SDBus Connect again...
TIWLAN: 0.057203: Try to SDBus Connect again...
TIWLAN: 0.057697: Try to SDBus Connect again...
TIWLAN: 0.058186: Try to SDBus Connect again...
TIWLAN: 0.058675: Try to SDBus Connect again...
TIWLAN: 0.059164: SDBus Connect Failed, Set Object Event !!

  • Lin,

    I am not much aware of WinCe but any idea what are these errors. It seems that it is not able to opwn some file and so connection to SDBus might be failing.

    TIWLAN: 0.056146: TIWL: Could not open image file, status=0xc001001b
    TIWLAN: 0.056493: Try to SDBus Connect again...
    TIWLAN: 0.056597: Try to SDBus Connect again...
    TIWLAN: 0.056705: Try to SDBus Connect again...
    TIWLAN: 0.057203: Try to SDBus Connect again...
    TIWLAN: 0.057697: Try to SDBus Connect again...
    TIWLAN: 0.058186: Try to SDBus Connect again...
    TIWLAN: 0.058675: Try to SDBus Connect again...
    TIWLAN: 0.059164: SDBus Connect Failed, Set Object Event !!

    Regards,

    Naveen