This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF-LAUNCHXL: local OTA fail due to signature file is missing in TAR (after progress reached to 99%)

Part Number: CC3220SF-LAUNCHXL
Other Parts Discussed in Thread: UNIFLASH

Hi,

I am working on local OTA and everything looks ok but at the end of local OTA reached upto 99% and it fails due to signature file is missing in TAR.

I am using uniflash version 1.0.22.3

Please refer attached image1 for the userFiles structure and image2 for the error screenshot which comes at last.

Please suggest.

Thanks and Regards,

Jasmin