Other Parts Discussed in Thread: UNIFLASH
We need to implement long range 5GHz connection (~10-15 km), we will use our own RF amplifier and antenna to reach needed RF power level.
Also to do this we need to increase acknowledgment timeout in PHY, because standard is ok for distance about 1,5 km .
UniFlash and SimpleLink API dose not provide such functionality, as I observe, but may be I miss something?
I notify on Simpllink API Sockoption for PHY level some options for transceiver mode :
- SL_SO_PHY_TX_INHIBIT_THRESHOLD
RAW socket, set WLAN Tx Set CCA threshold.
The values are based on SlTxInhibitThresholde
This options takes <b>_u32 as parameter
-SL_SO_PHY_TX_TIMEOUT
RAW socket, set WLAN Tx changes the TX timeout (lifetime) of transceiver frames.
Value in Ms, maximum value is 100ms
This options takes <b>_u32 as parameter
- SL_SO_PHY_ALLOW_ACKS
RAW socket, set WLAN Tx Enable\Disable sending ACKs in transceiver mode
0 = disabled / 1 = enabled
This options takes <b>_u32 as parameter
Are this option could help me to rich the aim? Or may be you can provide firmware with modified TX ack to value?