Other Parts Discussed in Thread: CC3135
Hi,
My customer requirement is using Wi-Fi device (server) as AP mode to receive up to 240 STAs (client)to get data stream like ADC sensor data,maybe 2 bytes at most, polling rate is 1 time per second.
I think I may have these options:
1. Use C3235 server with AT command demo code to config it as AP mode, so all STAs connect to server directly.
2. Use CC3235 server with AT command to config as STA mode then all STAs connect to same AP.
3. Use CC3135 with powerful Tiva MCU as AP mode, let STAs connect to it.
With these options, is that possible to have 240 STAs to connect? If not, what is the maximal connections we can have?
Thanks a lot.