Other Parts Discussed in Thread: CC3235SF, UNIFLASH
Hi E2E,
I'm testing CC3235MODASF and want to download a bin file through XDS which is on a LaunchPad, But XDS cann't connect to the target as shown in the pics below.
I connected the JTAG(4w), nRESET and UART0 to MSP432 or CC3235SF LaunchPad so as to VBAT1, VBAT2 and GND. As I know the SOP(2:0) had been pulled down with about 90kΩ resistances to configure 3235 in Functional development mode. In this mode, 4-pin JTAG is available to the developer.
I also tried to do this through UniFlash, unfortunately, it still doesn't work and came up with the same result.
Can you tell me how to flash the bin file to CC3235MODASF?
Thank you in advance.
Regards,
Siemin