Other Parts Discussed in Thread: ADS1220, CC3135, CC3120, BOOSTXL-ADS1219,
Hello,
I am thinking to develop BoosterPack which works with all Launchpad. It consist from an SPI display and ADS1220. I would like to use it with MSP430G2ET, MSP430F5529LP -that is not a problem- but would make sense to work with wireless Packs like MSP432P401R-CC3135. The problem is that the documentations of the booster connection of CC3135 is not understable: which line is free for use and which is used for communicating with processor, which is used only for programming and can be applied in normal use.
Could you help me with some reference about CC3135 and CC3120 connections??
Regards,
LAszlo