Other Parts Discussed in Thread: CC3120
Hi,
we are using CC3120MOD in a very low power device.
For this reason the connection to the WLAN (AP) and IP address acquisition (DHCP is used).
I tested some brands of AP (D-LINK, TP-LINK, MIKROTIK,...).
The time for WLAN connection is different for different brands, but for MIKROTIK is terrible - from 3.5 to 4.5 seconds.
For the other brands the time is under 3sec.
The type of connection policy ,which is used is "Auto", because the device is movable and can change the AP.
From AP point of view for fast connection DTIM time interval and Beacon time interval should be fast (DTIM = 1, beacon time interval - 100ms) to expect fast connection.
Can you suggest please, hoe to improve the connection time to the AP?
Best regards,
Ilian