I have a customer who is new to the wireless space and could use some design suggestions.
The application includes several nodes all communicating to one central node independently of any existing network.
A few initial questions from the customer:
1) How should the decision of 1 or 2 antennas be made?
2) Does a dual antenna module require a physical separation distance? (Some models of their device family are small- 6” x 6”)
3) What kind of certification has been done on these modules? What additional testing will they need to perform as the customer?
Appreciate any guidance!