Other Parts Discussed in Thread: TIDC-01005, UNIFLASH, CC3220S
Hi TI Wifi Experts,
I am working on bringing up TIDC-01005. first i have download and installed all the SDK match to the user guilde.
I loaded the Premade UniFlash ImageCreator Project and in Tera Term and I got:
[MQTT Thread] Connection to broker failed, Error code: -111 BRIDGE DISCONNECTION
#define SL_ERROR_BSD_ECONNREFUSED (-111L) /* Connection refused */
This is likely the eclipse broker is not active anymore. Therefore, I do the following:
1. Download a new der from mosquitto.org
2. Changed the download der file to "eclipsecert.der"
3. Download a new der from github.com
4. Changed the download der file to "digicertca.der"
5. Go to uniflash advance -> userfiles
6. add all the dummy and the two downloaded .der files
7. burn and program image again
8. complete provisioning and I receive the same error.
Can you let me know what I missed?
Thanks,
Shing