Other Parts Discussed in Thread: CC31XXEMUBOOST, UNIFLASH, , CC3135, CC3200
hardware platform:
CC31XXEMUBOOST & CC3100R1
software platform:
the latest version of the radio tool, (v1.2.5942) here is radio tool
CCS UniFlash
Question:
Now I want to use this radio testing tool to do some RF evaluation and testing of SimpleLink Wi-Fi CC3100R1. But, I can't connect this WiFi chip CC3100R1 with Radio Tool.The Radio Tool version is the latest.However, I can connect with CC3100R1 by CCS UniFlash.This radio testing tool cannot be connected to the Wi-Fi CC3100R1. Is it because the tool is not suitable for this CC3100R1 chip?
It is explained in the following figure.
1. cannot connect CC3100R1 by the Radio Tool
2. CC3100R1 Can be connected by CCS UniFlash
such as "GetVersion"
such as " List File System"
such as "Service Pack Programming"