Other Parts Discussed in Thread: CC3235MODS
Hi Camps,
Our customer is developing their system with CC3235MODAS2MONR. Customer is using the SimpleLink SDK APIs(drivers/net/wifi) and they plan to operate it in AP mode. in this case, customer would like to confirm if the following configurations are correct or not.
- Set Country Code for AP mode
- Customer is considering they should use sl_WlanSet(ConfigId, ConfigOpt, ConfigLen, pValues).
- ConfigId:SL_WLAN_CFG_GENERAL_PARAM_ID
- ConfigOpt:SL_WLAN_GENERAL_PARAM_OPT_COUNTRY_CODE
- ConfigLen: 2 ( byte)
- pValues: in the case of Japan, “JP”
- Set channel for AP mode after Setting Country Code
- Customer is considering they should use sl_WlanSet(ConfigId, ConfigOpt, ConfigLen, pValues), as well.
- ConfigId:SL_WLAN_CFG_AP_ID
- ConfigOpt:SL_WLAN_AP_OPT_CHANNEL
- ConfigLen: 1 ( byte)
- pValues: when this system I used in Japan, in the case of using 2.4GHz, 1-13. in the case of using 5GHz, 36,40,44,48,184,188,192,196.
Can I have your expert’s comments on this, please?
Especially, customer would like to confirm if pValues is correct or not. Customer is referring to the following URL.
it is the first time for customer to develop their system with CC3235MODS, therefore, regarding software side, if you will be able to share more helpful documents/URL, it will be really appreciated. And then, please teach us which sample code is better to understand CC3235MODS Wifi functions.
Best regards,
Miyazaki