Other Parts Discussed in Thread: UNIFLASH
Hello,
I am using TI controller CC3220SF for the development purpose. When I flash code through the Uniflash 6.3.0 in production Mode.
the controller behaves properly. but when i want to debug the application code in CCS 10.2 in debug mode gets the following Error.
Error connecting to the target:
(Error -1170 @ 0x0)
Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 9.3.0.00032)
I tried to flash the code in Development mode from the Uniflash software. and then tried to debug the code from the CCS 10.2 but the same Error Persist.
I have configured the Target configuration for cJTAG (1149.7 ) 4-pin standard mode. with default frequency 5.5 MHz.
ANY solution to resolve this issue will be appreciable.