Hi everyone,
I have integrated the wifi module(CC3100-Simple link)driver files with the stm32f1 micro-controller.To put the WIFI in some mode we should use the sl_start() API call and then sl_wlansetmode(ROLE_AP) to put in AP mode.
1.Using the API sl_start(0,0,0) returns 1 which is ROLE_UNKNOWN.
2.Then using the sl_wlansetmode(ROLE_AP) returns -100 which is SL_API_ABORTED (These error returns in all cases of ROLES)
Previous posts from forum asked to ensure that Service package is flashed or not,service package is flashed and then checked.
The same error still exists SL_API_ABORTED, while using the API sl_wlansetmode(ROLE_AP).
Kindly help me to resolve this issue.
Thanks & Regards,
Srigandeswaran S