Our current design is using the CC3220MODASF module, and I am checking to see if we can do a ‘drop-in’ with the CC3235MODASF. Everything looks the same except pins 25, 26, and 29. For the CC3235MODASF, these are ground pins. For the CC3220MODASF they are no-connects in our design (pin29 is required as NC; pin25-26 are analog outputs which are NCs). Can the CC3235MODASF have pins 25,25,29 as no-connects?