Other Parts Discussed in Thread: CC3200
I am attempting to use the parallel camera interface module on a CC3200-LAUNCHXL. It appears that it will not function without some board modification. In particular, I need I2C to configure the image sensor registers. However, the only SDA capable pin with external pull-ups on the board is pin 2 which is also the only pin the external camera clock can operate on. I can add a pull-up to some other pin that is capable of being configured as SDA, but I would rather not have to alter the board if I can help it.
Is there some way to use the parallel camera interface on the CC3200-LAUNCHXL that I am missing?
If not, is there another Wi-Fi SoC board that is capable of interfacing to an image sensor (I don't really have to use a CC3200. I just need a Wi-Fi SoC)?