This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHCC3235MOD: CC3235MODS on LaunchCC3235MOD board

Part Number: LAUNCHCC3235MOD
Other Parts Discussed in Thread: CC3235MODS, , CC3235MODSF, SYSCONFIG

Hello,

We are developing an application using CC3235MOD and would like to validate operation on CC3235MODS before purchasing the BoM for our application.

The application is working with LaunchCC3235MOD as delivered with CC3235MODSF. We have changed the module for CC3235MODS and added the serial SPI flash together with jumper resistor to connect it and power it.

How should we configure Code Composer (Sysconfig editor) ? Are there any specific hardware changes to make other than related to the Serial SPI flash.

  • Hi Chris,

    The only difference between the two modules is that the CC3235MODSF contains 1MB of exaction flash (XIP, parallel or on-chip), which is briefly explained in section 3 of datasheet. To use your application on the  CC3235MODS you will need to change linker file for execution from RAM as explained in this other post.

    Hardware wise there should be no difference on the LaunchCC3235MOD.

    Best Regards,

    Jessica