Other Parts Discussed in Thread: CC3220SF, , SYSCONFIG
Hi there, I've got a question about the pin mappings of the LAUNCHCC3220MODASF versus the pin mappings of the CC3220MODASM2MONR chip. I bought the standalone chip for a custom PCB, and also purchased the Launchpad that was listed as the development/evaluation board for this chip. Code Composer Studio recognizes the Launchpad as the CC3220SF, which is a different Launchpad model. The pin mappings for the Launchpad appear to match the pin mappings of the CC3220SF though, and I'm able to program the Launchpad without issue. The concern lies with flashing a program that runs on the Launchpad onto the CC3220MODASM2MONR chip. For example, a basic blinking LED program using GPIO_06 on the Launchpad uses pin 61, but on the standalone chip, GPIO_06 is pin 51 and pin 61 is a thermal ground pad.
How can I remedy this pin mismatching so I can flash programs that run on the Launchpad to the standalone chip without issue?