Hello
We have a very serious issue at our live customer demo site. Please check the exact statement as below.
Problem.
CC3235 is not going to connect with the router.
Test point.
1. Checked for application code it is working.
2. Check Wi-Fi 802.11 log-on sniffer device for this mac_address. It is not transmitting anything.
3. We have put sl_WlanPolicyGet API to test the network processor's health. If the response shows any error for the API then we have rebooted the MCU for testing. But its response is getting proper so the device is not going to reboot. (Not sure it is correct or not.)
4. Connection with Wi-Fi router is in Auto mode. So network processor should connect with the stored Wi-Fi profile automatically.
5. Our device has no option to check the UART log or JTAG.
We need your help to get resolve this problem.