Other Parts Discussed in Thread: CC3135
Hello Experts,
My customer is considering to use the CC3135MOD and they have inquiry FLASH SPI pins and TEST pins
of the CC3135MOD as follows;
---
In the CC3135MOD data sheet has miss match the input / output attributes (I/O TYPE) for FLASH SPI pins and TEST pins.
1.P10 Table 7-1. Pin Description and Attributes
2.P45 Figure 10-3. CC3135MOD Module Reference Schematic
As a pin number,With 13,14,15,17 FLASH_SPI pins,
It is a TEST pin of 48,49,50,52.
---
I Think that about FLASH SPI pin,
No.1 is writing from the CC3135 to 32-Mbit SFlash and No2. is writing from the external to 32-Mbit SFlash
(External SPI Programming) when FLASH SPI pins of the CC3135 are Hi -z stat.
About TEST pins, I have no idea.
Tell me please about this.
Best regards,
Y M