This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDC-01005: Import project error

Part Number: TIDC-01005
Other Parts Discussed in Thread: CC3220SF-LAUNCHXL

Hi, 

I installed the simplelink_sdk_wifi_plugin_4_20_00_10 and TIDC-01005 SW.

TIDC-01005 SW requires 3.6.0.0 but I couldn't find it. So I installed latest version.

And then I imported the wifi doorlock project in CCS but error is occured.

please let me know how to demo the wifi doorlock.

  • The project was done on CC3220.

    In order to move to a CC31xx you will need to create a project for your host and port the code yourself.

  • Hi, 

    I don't use CC31xx. My target is CC3220SF-LAUNCHXL.

    I also installed simplelink_cc32xx_sdk_5_20_00_06 previously.

    The reason I installed the SimpleLink WiFi pulg-in is because the default path is simplelink_sdk_wifi_plugin_3_60_00_00 when installing the example.

  • ok. the path to the tirtos projectspec was changed in the recent SDKs.

    Open the projectspec file in the tidc sw and look for "import spec" - you can either remove this line (and then you'll need add the tirtos project as dependency in the doorlock project) or change it to the following:

        <import spec="${COM_TI_SIMPLELINK_CC32XX_SDK_INSTALL_DIR}/kernel/tirtos/builds/cc32xx/release/ccs/tirtos_builds_cc32xx_release_ccs.projectspec"/>

    Once you change this, you should be able to import the project.