Hi,
I am using CC3235S launchxl kit. Board is restarting when I call a function PRCMHibernateEnter() to put the device into the hibernate mode. Same code is working fine with custom board. How can I put the Launchxl kit into the hibernate mode?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using CC3235S launchxl kit. Board is restarting when I call a function PRCMHibernateEnter() to put the device into the hibernate mode. Same code is working fine with custom board. How can I put the Launchxl kit into the hibernate mode?
Hi,
I'll get back to you by the end of this week regarding some sample to put the board into hibernate.
Hi Tejas,
Can you give me some more information on your issue? Can you provide code sample? What are the hardware differences between your board and the launchpad?
If the device is restarting after hibernate enter, that means a wakeup is occurring. Could you please use "PRCMHibernateWakeupCauseGet" to determine the cause of the wakeup?