Other Parts Discussed in Thread: WL1805MOD
Dear Support
I get approved antenna list from support.
I can not find ANT016008 in the TDK Homepage.
But In the TDK Home page there are
.
Are they approved antenna?
Best regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tadanori,
The antennas you listed are the single-band variants, which are approved for WL18MODGB modules.
The dual-band variant is approved for WL18MODGI modules.
BR,
Seong
Dear Seong
The antenna you linked is that one not recommended for new designs by Maker(TDK)..
If I use the single-band , can I use them?
Hi Tadanori,
If you only need 2.4GHz, perhaps you should consider using the WL1805MOD instead as it is lower in cost. See table 2-1 in the WL8 Getting Started Guide.
If you plan to use a single-band 2.4GHz chip antenna, you can use any chip antenna with a gain that does not exceed 3.2dBi.
BR,
Seong