Hi, I have some troubles with the realization of antenna switching using auto_selection mode with one GPIO line. I am using your network terminal example to test the automatic mode selection. Earlier I asked this forum about, Is it possible to use auto_mode selection with only 1 GPIO? Here is the link https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/1059695/cc3235modsf-questions-about-antenna-selection-usage
It seems that it is possible due to the reply. SDK version is 5.30.00.08. Below, you can see the questions with which I am having problems:
1) There are no problems switching manually with a single GPIO line. When I try to change the mode of antenna selection from Fixed one to Auto-select one using just 1 GPIO line, of course, disconnected from any Acces Point, it gives a SL_ERROR_INVALID_OPCODE error. Why is it happen?
2) In your example of auto_selection mode your engineers used the structure of 2 GPIOs. What is the exact model of the 2 GPIOs switch that is used in your reference design?
Best Regards, Alex.